LUFP7. Parameters are set using ABC configuration software. This software comes with the LUFP7 gateway. The LUFP7 is not specifically designed to be used with any particular product. It is a basic gateway that required configuration to allow Profibus to access registers for reading and writing using Modbus. This LUFP7 is recommended for use with the ATV31 and ATS48 products in their respective catalogs. It will operate with other Modbus compatible devices as well.
Reviewed 6/2011
CTA-ID : 2020346
Reviewed 6/2011
CTA-ID : 2020346
Released for:Schneider Electric USA