{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the replacement armature and magnet kit for the Class 8502 or Class 8536 Type SF__ device.
Issue:
Part # for armature replacement and magnet kit for the Class 8502 or Class 8536 Type SF device.

Product Line:
NEMA Starters​​​​​​​

Environment:
NEMA Type S Motor Starters (8536 8736 8606)
​​​​​​​

Resolution:
Use part number 31091-514-50.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.