{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What enclosures are available to mount an individual QBL, QDL, QGL, or QJL circuit breaker?
Issue:
Product Availability

Product Line:
Enclosures

Resolution:
Available enclosures include:
1) Q22200NS (NEMA 1 surface; 2 pole, 200 ampere maximum)
2) Q22200NRB (NEMA 3R; 2 pole, 200 ampere maximum)
3) Q23225NF (NEMA 1 flush; 2 and 3 pole, 225 ampere maximum)
4) Q23225NS (NEMA 1 surface; 2 and 3 pole, 225 ampere maximum)
5) Q23225NRB (NEMA 3R; 2 and 3 pole, 225 ampere maximum)
The enclosures marked for use with the QBL, QDL, QGL, or QJL breakers are designated series E05. For retrofitting these breakers into existing series E03 or earlier enclosures, restrictions regarding short circuit current ratings apply. The following statement is on the wiring diagram of the series E01 and E03 enclosures: "The short circuit rating of this enclosure is equal to the interrupting rating at the supply voltage marked on the circuit breaker installed, but not to exceed 42,000 RMS Symmetrical Amperes at 240Vac. Replacement circuit breakers must have an interrupting rating equal to or greater than that of the circuit breaker originally installed".

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: