{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Square D offer a keyed 30 mm corrosion resistant selector switch?
Issue:
Corrosion resistant availability of 30mm keyed selector switches

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony 30 mm 9001 K/SK Push Buttonss

Resolution:
No, the 30 mm 9001SKS corrosion resistant operators do not have a keyed option. Customers must select the 9001K non corrosion resistant type to obtain keyed operation.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: