{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the Difference Between the Two Coils on the 8903 Mechanically Held Lighting Contactor?
Issue:
There are two different part numbers for the latch and unlatch coils.

Product Line:
NEMA Contactors and Starters

Environment:
8903 Lighting Contactors

Resolution:
One is a latching coil and is continous duty rated. The other is an unlatch coil and is not continuous duty rated.

Schneider Electric USA