undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
I am doing an insulation test on 100 Ft of 5000A busway. What is the minimum megohm reading from phase to phase, phase to neutral, and phase to ground?
Issue:
Insulation test on 100ft of a 5000A busway.

Product Line:
I-Line

Environment:
North America products

Cause:
Test

Resolution:
Regardless of the busway amperage, the minimum acceptable megohm reading is 100 divided by the length of the run in feet. (100 / feet). For example, if the busway run is 50 feet long, the minimum acceptable reading would be 100 / 50 = 2 megohms.
 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top