{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a resistor capacitor surge suppressor available for the Class 8910 Type DP or Type DPA contactor?
Issue:
Is there a resistor capacitor surge suppressor available for the Class 8910 Type DP or Type DPA contactor?

Product Line:
Nema and Definite Purpose and Starters

Environment:
North American Products

Resolution:
Not specially designed for the Class 8910 but the 9999ST1 which is used for the Class 8502 & Class 8536 starters will work. However, this is for 120 volt control coils only and will require panel mounting.

Schneider Electric USA