{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are replacement or field assembly NEMA 3R enclosures available for the Class 8903 Type SP lighting contactors?
Issue:
Is there a NEMA 3R replacement enclosures for the Class 8903 Type SP lighting contactors?

Product Line:
Class 8903 Type S Lighting Contactors

Environment:
NEMA Starters and Contactors accessories

Resolution:
Yes, for 60 amp non-combination mechanically and electrically held contactors all pole arrangements will use part number 9991SDH1.

Schneider Electric USA