{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the catalog number for the knob only for a ZB4 / ZB5 illuminated selector switch?
Issue:
Separate part number for ZB4 / ZB5 selector switch knob.

Product Line:
22mm Harmony Push Buttons

Environment:
Harmony XB4/XB5 Selector Switch

Resolution:
We don`t offer the selector switch knobs as a replacement part. They must get the entire operator head.

Schneider Electric USA