{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is the ZCKE04 Head Replaceable?
Issue:
Replacement for a defective ZCKE04 limit switch head

Product Line:
Heavy Duty / Industrial Limit Switches

Environment:
XCKJ Operating Heads

Resolution:
No. The body and head are available only as a complete unit (less the lever arm). Order ZCKJ404 for non plug-in housing or ZCKJ4104 for plug-in housing.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.