{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for an auxiliary contact for 30 and 60 amp Class 8903 Type S lighting contactor?
Issue:
Auxiliary contact for 8903 Type S 30 and 60amp.

Product Line:
NEMA Contactors and Starters

Environment:
8903 Type S Lighting Contactors

Resolution:
Select External Auxiliary Contact(s) from table below:

(1) normally open, field convertible 10 amp contact - 9999SX6
(1) normally closed, field convertible 10 amp contact - 9999SX7
(1) normally open, overlapping field convertible 10 amp contact - 9999SX9
(1) normally closed, overlapping field convertible 10 amp contact - 9999SX10
(1) normally open and (1) normally closed, isolated field convertible 10 amp contacts - 9999SX8

(1) normally open, non-field convertible 10 amp contact - 9999SX13
(1) normally closed, non-field convertible 10 amp contact - 9999SX14
(1) normally open, overlapping non-field convertible 10 amp contact - 9999SX15
(1) normally closed, overlapping non-field convertible 10 amp contact - 9999SX16
(1) normally open and (1) normally closed, isolated non-field convertible 10 amp contacts - 9999SX17

(1) normally open, non-field convertible internal 3 amp contact - 9999SX11
(1) normally closed, non-field convertible internal 3 amp contact - 9999SX12

Schneider Electric USA