{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Does Square D/Schneider Electric offer Transformers rated for marine type applications?

Issue:

Marine ratings for Transformers

Product Line

LV Transformers

Environment:

Applies to LV Transformers by SquareD/Schneider Electric.

Cause:

Special requirements apply for Transformers built for shipboard and marine use

Resolution:

Yes. Once the customer supplies the average and maximum ambient temperatures into which the Transformer will be applied, Square D/Schneider Electric will design, build, and nameplate a Transformer to IEEE Standard 45.

Schneider Electric USA