{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can ANY of the QO OEM mounting bases be converted to have a main breaker?
Issue:
Are the QO OEM mounting bases convertible to main breaker style?

Product Line:
OEM Mounting Bases for miniature breakers

Resolution:
NOTE:
CANNOT EXCEED THE AMPERE RATING OF THE OEM MOUNTING BASE.

The following main lug OEM mounting base catalog numbers can be field converted to a main breaker OEM mounting base by using a QOM1-VH or QOM2-VH main circuit breaker kit depending on the part number of the interior. The QOM1-VH kits range from 50 - 125 A and QOM2-VH kits range from 100 - 225 A. They can be field installed to replace the factory installed main lugs. The final acceptance of this component is dependent upon its installation and use in complete equipment submitted to Underwriters Laboratories, Inc. by the OEM.
OEM InteriorAmpere RatingMain BreakerCat. # of max MB
QON112L125I125AQOM1-VHQOM125VH
QON11224L125I125AQOM1-VHQOM125VH
QON116L125I125AQOM1-VHQOM125VH
QON11624L125I125AQOM1-VHQOM125VH
QON120L125I125AQOM1-VHQOM125VH
QON124L125I125AQOM1-VHQOM125VH
QON132L125I125AQOM1-VHQOM125VH
QON12024L125I125AQOM1-VHQOM125VH
QON142L225I225AQOM2-VHQOM2225VH
Main Breaker FrameAmpere RatingFor Convertible LC with Mains RatingCat. No.Lug Wire Size (AWG/kcmil)
QOM1-VH50A100A-125AQOM50VH12-2/0 Al or Cu
60A100A-125AQOM60VH
70A100A-125AQOM70VH
80A100A-125AQOM80VH
90A100A-125AQOM90VH
100A100A-125AQOM100VH
110A125AQOM110VH
125A125AQOM125VH
QOM2-VH100A150A-225AQOM2100VH4-300 Al or Cu
125A150A-225AQOM2125VH
150A150A-225AQOM2150VH
175A200A-225AQOM2175VH
200A200A-225AQOM2200VH
225A225AQOM2225VH

Schneider Electric USA

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: