{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can QO riser panels be mounted so that the gutter is on the left hand side?
Issue:
Gutter position of riser panel

Product Line:
QO Load Centers

Resolution:
Yes, these load centers can be rotated 180 degrees so that the gutter is on the left side. This will put the main lugs at the bottom of the load center, as shown below:
QO upside down riser panel

Schneider Electric USA