{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for a QC816F200C, series M01?
Issue:
Repair parts part number for a QC816F200C, series M01

Product Line:
Combination Service Entrance Devices (CSED), QO Load Centers, Meter Main

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056167850 (includes latch)
Load Center Cover - 4056157550 (includes hinges and latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056173701
Dead Front Interior Trim Mounting Screws - 4020513001K (contains 10 screws; only 3 screws are required)
Load Center Interior - 4056161751 (does not include main breaker nor feed-thru lugs)
Load Center Interior Mounting Screws - (6) 2153217161
Main Breaker - QOM2200VH
Mounting Hardware - (2) 2342702001 keps nuts and (1) 2142717480 screw
Feed Thru Phase Lugs - (2) 4025116051
Mounting Keps Nuts - (2) 2342702001
Meter Base Assembly - 4056190150 (includes meter base, line side lugs, line and load side meter jaws, meter jaw blade guides, and load side busbars)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Keps Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: