{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the mechanical and electrical durability of NEMA Starters and Contactors?
Issue:
Mechanical and electrical life in number of cycles for the NEMA contactors and starters

Product Line:
NEMA Contactors and Starters

Environment:
NEMA and Definite Purpose Contactors and Starters

Cause:
Needs the mechanical and electrical life in number of cycles for the NEMA contactors and starters.

Resolution:
The life expectancy is based on the NEMA size of the device as follows:
NEMA Size - Mechanical Operations - Electrical Operations
00 - 6,000,000 - 600,000
0 - 10,000,000 - 1,000,000
1 - 10,000,000 - 1,000,000
2 - 10,000,000 - 1,000.000
3 - 5,000,000 - 500,000
4 - 3,000,000 - 300,000
5 - 2,000,000 - 200,000
6 - 1,500,000 - 150,000
7 - 500,000 - 50,000

Schneider Electric USA

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.