Issue:
Do the GV3 manual starters and protectors provide single phase sensitivity?
Product Line:
IEC Contactors and Starters
Environment:
Tesys GV3 Manual Starters
Resolution:
Yes, however you must verify that the device in question is suitable for the load to be controlled. Additionally, because these devices have single-phase sensitivity, provisions must be made to ensure nuisance tripping does not occur due to the single phase application. This can be accomplished by wiring the device so that the full motor current passes thru all three legs of the GV.
Do the GV3 manual starters and protectors provide single phase sensitivity?
Product Line:
IEC Contactors and Starters
Environment:
Tesys GV3 Manual Starters
Resolution:
Yes, however you must verify that the device in question is suitable for the load to be controlled. Additionally, because these devices have single-phase sensitivity, provisions must be made to ensure nuisance tripping does not occur due to the single phase application. This can be accomplished by wiring the device so that the full motor current passes thru all three legs of the GV.