{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the Class 8536 Type S starters suitable for use for group motor applications?
Issue:
Can the Class 8536 Type S starters be used on group motor applications?

Product Line:
Nema and Definite Purpose and Starters

Environment:
Type S Contactors and Starters

Cause:
Needs the know if the Class 8536 Type S starters suitable for use for group motor applications.

Resolution:
No, these NEMA rated devices provide no short circuit protection and therefore are not suitable for use for group motor.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.