Issue:
Is it possible to use the QO 2 pole GFI in a 120Vac and 240Vac system?
Product Line:
Miniature Molded Case Circuit Breakers
Resolution:
Yes, as long as the neutral for the 120 Vac loads is connected to the neutral terminal on the breaker and the pigtail is connected to the neutral bar in the panel.
EXCEPTION: The QO260GFI does not have a load neutral connection, and is therefore not viable for this application.
Is it possible to use the QO 2 pole GFI in a 120Vac and 240Vac system?
Product Line:
Miniature Molded Case Circuit Breakers
Resolution:
Yes, as long as the neutral for the 120 Vac loads is connected to the neutral terminal on the breaker and the pigtail is connected to the neutral bar in the panel.
EXCEPTION: The QO260GFI does not have a load neutral connection, and is therefore not viable for this application.