Search FAQs
Can the EZM125QOA tenant breaker adapter kit be used in any MP Meter-Pak meter centers?
Issue:
Product features
Product Line:
MP Meter-Pak metering
Resolution:
The EZM125QOA adapter is suitable for use ONLY in the following MP METER-PAK meter centers to convert a bolt on Q-Frame tenant circuit breaker position to accept a plug-on style QO, QO-VH, or QOH, 2 pole, 40 - 125 A tenant circuit breaker: catalog numbers MPL32225, MPL53225, and MPL64225.
Product features
Product Line:
MP Meter-Pak metering
Resolution:
The EZM125QOA adapter is suitable for use ONLY in the following MP METER-PAK meter centers to convert a bolt on Q-Frame tenant circuit breaker position to accept a plug-on style QO, QO-VH, or QOH, 2 pole, 40 - 125 A tenant circuit breaker: catalog numbers MPL32225, MPL53225, and MPL64225.
Released for:Schneider Electric USA
Explore more
Product:
Range:
Explore more
Product:
Range: