{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the significance of the suffix SW1, SW2, SW3, SW4 or SW6 on Square D/Schneider Electric Transformers such as 75T145HDITSW1?
Issue:
Suffixes on Square D/Schneider Electric Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformer options are often denoted by appropriate suffixes at the end of the catalog number


Resolution:
The SW(_) suffix denotes the Transformer has thermal switch(s) in the coil(s) of the Transformer. The standard switch is a Normally Closed set of contacts that will change state at 180C. Where two switches are installed in a coil, the second switch is a Normally Closed set of contacts set to 200C).
SW1 denotes one switch in the center coil of a three-phase transformer.
SW2 denotes one switch in each coil of a single-phase transformer, or two switches in the center coil of a three-phase transformer.
SW3 denotes one switch in each coil of a three-phase transformer.
SW4 denotes two switches in each coil of a single-phase transformer.
SW6 denotes two switches in each coil of a three-phase transformer.


CTA-ID : 2026729

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: