{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the padlocking attachment for a QB, QD, QG, QJ breaker?
Product Line:
Circuit Breakers
PowerPact Q

Environment:
Electrical Distribution Equipment

Resolution:
QBPA is for locking in the ON or OFF position. QBPAF is for locking in the OFF position only. Both are fixed attachment. There are no removable attachments for the Q-frame.

Intended for use with the QBMIK Mechanical Interlock Kit:
QBPAL is for locking in the ON or OFF position & mounted on left side of the breaker.
QBPAFL is for locking in the OFF position & mounted on the left side of the breaker.
 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: