{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the torque requirement for the lugs on a 400A main lug and neutral I-line panel?
Issue:
Torque specs for I-Line panel lug

Product Line:
Panelboards

Environment:
I-Line

Cause:
Installation and maintenance

Resolution:
For 3/8`` screw it is 340 in-lbs. For 1/2`` screw it is 450 in-lbs.


 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: