{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the GV2ME__, GV2P__, or GV3P__ IEC manual starters available enclosed?
Issue:
GV2ME**, GV2P**, GV3P** enclosure

Product Line:
Tesys GV Manual Starter and Protectors

Environment:
TeSys™ GV Manual Starters and Protectors

Resolution:
No, however we offer enclosures for field installation for the GV2ME. There is no enclosure offered by Telemecanique for the GV_P__, however we do offer through the door operating mechanisms to use in a separate enclosure. Please see tables below for selection.

GV2 Enclosures:
DescriptionMountingRatingCatalog Number
Enclosures for GV2M with or without accessories (max of 1 accessory on left and right) Enclosures are not UL / CSA listedSurfaceNEMA1, IP41GV2MC01
IP55GV2MC02
FlushNEMA1, IP41GV2MP01
IP55GV2MP02
Flush with reduced width (max 1 accessory on right)NEMA 1, IP41GV2MP03
IP55GV2MP04

GV2P Through the door operators:
ApplicationCatalog Number
NEMA 1/12, black with trip indicationGV2APN01
NEMA 1/12, red/yellow with trip indicationGV2APN02
NEMA 3R/4/4X red/yellow without trip indicationGV2APN04

GV3P Through the door operators:
ApplicationCatalog Number
NEMA 1/12, black with trip indicationGV3APN01
NEMA 1/12, red/yellow with trip indicationGV3APN02
NEMA 3R/4/4X red/yellow without trip indicationGV3APN04

Schneider Electric USA