{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are NQ enclosures available ``free-standing``?
Issue:
Can an NQ enclosure be floor mounted rather than wall mounted?

Product Line:
NQ Panelboards

Environment:
Panelboard enclosures sold and supported in the USA

Cause:
Freestanding panelboard enclosures

Resolution:
A freestanding enclosure with base channels is available. Base channels can be selected in Product Selectors. The Base Channels will extend out the front and the back and will be welded to the bottom of the enclosure.  Another option is for installer can fabricate something in the field to make the panelboard freestanding.
Note that these are only available on indoor Nema 1 and Nema 12 enclosures.  They are not available or recommended for Nema 3R/12 outdoor enclosures.

Schneider Electric USA