{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the standard terminal lug data (or wire size) for all the QMB/QMJ branch switches?
Issue:
product design features

Product Line:
QMB and QMJ branch switches

Resolution:
See the tables below for the terminal lug data (or wire size) for ALL the current series design QMB/QMJ branch switches.
NOTE: The QMB/QMJ branch switches come with standard mechanical lugs that accept Cu or Al wire. There are NO alternate lugs available to allow for either larger wire or more quantity of wires. The only potential optional lug would be a compression lug. See the current QMB catalog section or each switch wiring diagram for the available compression lugs.

QMB and QMJ Table

Schneider Electric USA

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product:
move-arrow-top