{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

How can we help you today?

Are the MPZ Mini Power Zone rated for outdoor use?

Issue:
Mini Power Zone NEMA rating

Product Line:
Square D Transformers

Environment:
Transformer configuration

Resolution:
Yes, as shown in the Digest, the Mini Power-Zone Transformer Indoor/Outdoor Packaged Power Supply has a NEMA 3R rated enclosure which is suitable for both indoor and outdoor locations, and they are suitable for service entrance use.


Schneider Electric USA