{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is required to field install an ON-OFF push button on the Class 8903 Type LG__ lighting contactor?
Issue:
Is the bracket needed to field install an ON-OFF push button in the class 8903 type LG__ lighting contactor?

Product Line:
NEMA Contactors and Starters

Environment:
Class 8903 Type LG___ contactor

Resolution:
9999SA10 cover mounted control station and 9999BLX mounting bracket. The 3-wire control also requires the use of a power pole to function as the holding circuit contact.

Schneider Electric USA