{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do ANY of the Combination Service Entrance Devices (CSED) come with a neutral bonding screw and are CSED UL Listed for use as Service Equipment?

Article available in these languages: Spanish

Issue:
Current design features

Product Line:
Combination Service Entrance Devices

Environment:
Service Entrance rating

Cause:
Application Code requirement

Resolution:
CSED = Combination Service Entrance Devices


None of the CSED are supplied with neutral bonding screws. ALL the CSED are UL listed for, and marked as,  "Suitable ONLY For Use As Service Equipment".  Therefore, the main neutral is factory bonded to the enclosure as standard.

Schneider Electric USA

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: