Issue:
Selection
Product Line:
HOM Load Center
Resolution:
Yes, there are optional, field installed neutral lugs that can be installed on most Homeline load centers. They could also be installed on an equipment ground bar. The options are LK70AN (#12 - 2 AWG Al or #14 - 4 AWG Cu), LK100AN (#6 - 2/0 AWG Al/Cu), LK125AN (#14 - 2/0 AWG Al/Cu), LK150AN (#2 - 3/0 AWG Al/Cu) or LK225AN (#4 AWG - 300 kcmil Al/Cu).
Selection
Product Line:
HOM Load Center
Resolution:
Yes, there are optional, field installed neutral lugs that can be installed on most Homeline load centers. They could also be installed on an equipment ground bar. The options are LK70AN (#12 - 2 AWG Al or #14 - 4 AWG Cu), LK100AN (#6 - 2/0 AWG Al/Cu), LK125AN (#14 - 2/0 AWG Al/Cu), LK150AN (#2 - 3/0 AWG Al/Cu) or LK225AN (#4 AWG - 300 kcmil Al/Cu).
Released for:Schneider Electric USA
Issue:
Selection
Product Line:
HOM Load Center
Resolution:
Yes, there are optional, field installed neutral lugs that can be installed on most Homeline load centers. They could also be installed on an equipment ground bar. The options are LK70AN (#12 - 2 AWG Al or #14 - 4 AWG Cu), LK100AN (#6 - 2/0 AWG Al/Cu), LK125AN (#14 - 2/0 AWG Al/Cu), LK150AN (#2 - 3/0 AWG Al/Cu) or LK225AN (#4 AWG - 300 kcmil Al/Cu).
Selection
Product Line:
HOM Load Center
Resolution:
Yes, there are optional, field installed neutral lugs that can be installed on most Homeline load centers. They could also be installed on an equipment ground bar. The options are LK70AN (#12 - 2 AWG Al or #14 - 4 AWG Cu), LK100AN (#6 - 2/0 AWG Al/Cu), LK125AN (#14 - 2/0 AWG Al/Cu), LK150AN (#2 - 3/0 AWG Al/Cu) or LK225AN (#4 AWG - 300 kcmil Al/Cu).
Released for:Schneider Electric USA