{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the F-Line contactors rated to break DC voltages?
Issue:
Tesys F DC voltage contact rating

Product Line:
Contactors and Starter - IEC

Product Line:
Tesys F Line Contactors and Accessories

Resolution:
Yes, 125 VDC per pole which means that through a four pole device breaking 500 VDC is possible by wiring all four power poles in series. However, be aware that the device current ratings will differ according to the number of poles in series and the type of application.

Devices are suitable but not UL Listed for DC applications.

See pages 28 through 31 of the attached link (8502CT9901R5/03)

Schneider Electric USA