Issue:
Do you have an alternative way to mount the 9999RR04?
Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters
Environment:
Class 9999 Accessories
Resolution:
The 9999RR04 is designed to mount directly on the right side of the overload without a bracket. However, in order to keep from adding width to the overload the remote reset module can be mounted to the top of the overload using the 9999RB34 bracket.
Do you have an alternative way to mount the 9999RR04?
Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters
Environment:
Class 9999 Accessories
Resolution:
The 9999RR04 is designed to mount directly on the right side of the overload without a bracket. However, in order to keep from adding width to the overload the remote reset module can be mounted to the top of the overload using the 9999RB34 bracket.