{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Can a QOM2-VH breaker installed in a QOM22225NF, QOM22225NS, or QOM22225NRB enclosure be backfed and how does the breaker install in the enclosure?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QOM Circuit Breaker Enclosures

Resolution:
The QOM2 Enclosures are not marked for line and load, which means the incoming service wires can be connected to either the top lugs or the bottom lugs. BUT the local code authority may require the installer to mark the enclosure to designate the line and load side lugs.
See the attached video for how the QOM2-VH breakers install into the QOM2 Enclosures.

MAKE SURE TO FOLLOW ALL INSTRUCTIONS THAT COME WITH THE ENCLOSURE AND/OR QOM2-VH BREAKERS.
NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: