{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the X1 and X2 terminals on the ZBVB1 LED Light Module? Are they polarity sensitive?
Issue:
Identify the terminals on a 22mm light module

Product Line:
XB4 Pilot lights

Environment:
22 mm Push Button Operators

Cause:
Installing a ZB light module

Resolution:
X1 and X2 are the wiring terminals. They are not polarity sensitive.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.