Issue:
Repair parts
Product Line:
CSED
Repair:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Rainproof Cap - 4056115803 (top cap that covers the top endwall of the device)
Rainproof Cap Mounting Screws - (2) 2142717161
Meter Cover Assembly - 4056127952
Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only two are required)
Utility Pullbox Cover - 4056133952 (Iincludes cover latch)
Load Center Cover Assembly - 4056128052 (includes hinges)
Load Center Cover Mounting Rivet - (4) 2430315290
Dead Front Interior Trim - 7329421801
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one is required)
Load Center Interior - 4056127652 (does not include main breaker)
Load Center Interior Mounting Screws - (5) 2142217101
Main Breaker - HOM2200
Main Breaker Retaining Hardware - 4056132701 (hold down strap that straddles the main breaker), 4056152501 (clamp), 4056152601 (spacer), and 2159417721 (screw). The clamp, spacer, and screw are used on the line side of the main breaker.
Meter Base Assembly - 4056149452 (includes load side meter jaws and load side lugs; load side meter jaw blade guides not included)
Meter Jaw - (2) 7329794850 (load side meter jaws are included in meter base assembly)
Meter Jaw Mounting Keps Nut - (2) 2342702001 (load side meter jaw mounting keps nuts are included in meter base assembly)
Meter Jaw Blade Guide - (4) 4052761901
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.
Released for:Schneider Electric USA
Issue:
Repair parts
Product Line:
CSED
Repair:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Rainproof Cap - 4056115803 (top cap that covers the top endwall of the device)
Rainproof Cap Mounting Screws - (2) 2142717161
Meter Cover Assembly - 4056127952
Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only two are required)
Utility Pullbox Cover - 4056133952 (Iincludes cover latch)
Load Center Cover Assembly - 4056128052 (includes hinges)
Load Center Cover Mounting Rivet - (4) 2430315290
Dead Front Interior Trim - 7329421801
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one is required)
Load Center Interior - 4056127652 (does not include main breaker)
Load Center Interior Mounting Screws - (5) 2142217101
Main Breaker - HOM2200
Main Breaker Retaining Hardware - 4056132701 (hold down strap that straddles the main breaker), 4056152501 (clamp), 4056152601 (spacer), and 2159417721 (screw). The clamp, spacer, and screw are used on the line side of the main breaker.
Meter Base Assembly - 4056149452 (includes load side meter jaws and load side lugs; load side meter jaw blade guides not included)
Meter Jaw - (2) 7329794850 (load side meter jaws are included in meter base assembly)
Meter Jaw Mounting Keps Nut - (2) 2342702001 (load side meter jaw mounting keps nuts are included in meter base assembly)
Meter Jaw Blade Guide - (4) 4052761901
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.