{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do the LA9TFD32 and LA9TFD80 IEC control power transformer Insta-kits include fuses?

Issue:
What are the fuses in the Insta-kits control power transformer included?

Product Line:
Instakits accessories

Environment:
Applies to Enclosed TeSys D combination starters

Cause:
Fuse needs to be added or replaced

Resolution:
The Class CC rejection type primary fuses and the non-rejection secondary type fuses are provided.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: