{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a sensor that meets NEMA 7 & 9 explosion proof class 1 or II ?
Issue:
Looking for explosion proof rated sensors

Product Line:
Sensors

Environment:
Telemecanique Sensors

Resolution:
Telemecanique does not offer an explosion proof sensor that meets NEMA 7 gases (class1) or NEMA 9 for dusts (class II) . Try Acculex or Baumer for proxs that meet the NAMUR standard.

Schneider Electric USA