{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the recommended fuses for use with Control Transformer Kit, 9999 CPT1D3?
Issue:
Transformer fusing

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric


Cause:
Overcurrent protection is often required for Industrial Control Transformers

Resolution:

For the 208V primary, 1A fuses are recommended, with a maximum rating of 1.20A permitted using the 250% rule of NEC450.3. Please note the fuses are to be 600V maximum, 1-1/2 x 13/32`` Class CC rejection type, time delay fuses (Bussmann Type FNQ-R or equivalent). Qty (2) are required. On the 120V secondary side, a 1.25A fuse is recommended, with a maximum rating of 1.39A permitted according to the 167% rule of NEC 450.3. Provisions are for qty (1) fuse, which must be 1-1/2 x 13/32``, non-rejection type fuse (Bussmann type FNQ or equivalent).


 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top