{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the 30 mm LED`s now coming standard with super bright bulbs?
Issue:
LED Type on the 30mm operators

Product Line:
Push Buttons and Operator Interface

Environment:
9001 Type K Operators

Resolution:
9001KM35LR, 9001KM35LG and 9001KM35LY that operated on 24-28Vac/dc and the 9001KM38LR, 9001KM38LG, 9001KM38LY that operate on 120Vac/dc are considered Super bright and come standard this way.

Schneider Electric USA