Product Line:
Safety Switch
Environment:
Heavy Duty Safety Switch
Resolution:
The parts listed here are the only field replaceable parts.
Safety Switch
Environment:
Heavy Duty Safety Switch
Resolution:
The parts listed here are the only field replaceable parts.
- Line base assembly - 4055218850 (3 required; arc suppressor assembly not included)
- Load base assembly - 4055219050SEL (3 required)
- Arc suppressor assembly - 4051270850 (3 required)
- Lug Assembly - 4025113650 (1 required per base assembly)
- Line base phase insulator - 4051201401 (2 required)
- Load base phase insulator - 4055219101 (2 required)
- Line & load base mounting screws - 4020600901 (2 required per base assembly)
- Handle assembly - 4051217251
- Vault handle - 4051219450SEL
- Handle knob kit - 4028343550
Released for:Schneider Electric USA