undefined [object Object]
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the NF panelboards be used on a 480V 3PH 3W system?

Article available in these languages: Spanish

Issue:
Application on 3w system

Product Line:
Panelboards

Environment:
NF

Cause:
Use 4w panel on a different voltage

Resolution:
Yes, ONLY if the panel is being fed from a 480Y/277 V system upstream and they are simply not pulling the neutral conductor to the NF interior. 2 pole and 3 pole breakers can be used.

Note: The NF panel CANNOT be used on a 3ph, 3w delta system. The EDB or similar branch breakers are not rated for 480 V to ground.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: