Search FAQs
What size primary fuses (Class E type) are needed for a 1500kva, 4160v to 277/480v Liquid Filled Transformer? The fuses are for an HVL ahead of the transformer.
Issue:
What is the size of the primary fuse required for a 1500 KVA, 4160V to 277/480V liquid filled medium voltage transformer?
Product Line:
Medium voltage transformer
Environment:
Installation/specification
Resolution:
A 250E fuse will be required.
What is the size of the primary fuse required for a 1500 KVA, 4160V to 277/480V liquid filled medium voltage transformer?
Product Line:
Medium voltage transformer
Environment:
Installation/specification
Resolution:
A 250E fuse will be required.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: