{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the short circuit current rating for a 8903L and 8903LX?
Issue:
SCCR rating for 8903L Type L and Type LX

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8903 Type L and LX Multipole Lighting Contactors

Resolution:
The short circuit rating when protected by a fusible disconnect with 30A RK5 fuses is 100,000AIC. When it is protected by a suitable 25A thermal magnetic circuit breaker the ratings are: at 240V - 22,000; at 480V - 14,000.

Schneider Electric USA