{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the differences between a 9422A1 and a 9422A2 handle?
Issue:
What is the rating on a 9422A1 and A2 handle?

Product Line:
Operating Mechanism and Handle

Environment:
Class 9422 Type A1 and A2

Resolution:
The A1 handle is painted and rated NEMA 1, 3, 3R, 4 (sheet steel) and 12. The A2 handle has these same ratings plus NEMA 4/4X and is stainless steel.

Schneider Electric USA