Search FAQs
What are part numbers for an NQ/NQOD and NF Directory card holder and pouch?
Issue:
What is the circuit directory card and stick on pouch for NQ/NQOD and NF panelboards?
Product Line:
Panelboards
Environment:
Products sold in the United States
Cause:
Identification
Resolution:
The plastic pouch Square D offers is 8003115901 and the standard 42 circuit directory card is 8003115801. Note that the directory card is printed on one side with circuits numbered odd/even, that is, the left column of breakers number 1-41 odd, and the right column numbered 2-42, even. On the other side, the directory card is numbered sequentially, with the left column of circuits numbered 1-21 and the right column 22-42.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: