{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a DSL206 be used to replace a DS206?
Issue:
DSL206 used to replace DS206.


Product Line:
LVDO

Environment:
North America Products

Cause:
It is typically acceptable to substitute a circuit breaker with higher interrupting ratings for one with lower interrupting ratings, if they are otherwise alike in other characteristics. 

Resolution: 

NOTE:  DS and DSL circuit breakers are obsolete.  No, a DSL206 cannot replace a DS206 circuit breaker because the DSL206 is eight inches deeper than the DS206 due to the limiters located at the back of the device. 

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
move-arrow-top