{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are finger safe covers available for the LA/LH breakers?
Issue:
Do LAL breakers have finger-safe lug covers?

Product Line:
Circuit Breakers

Resolution:
LCA1A is a finger safe cover for the LA/LH breaker. There are 2 lug covers in the kit - one for each end of the breaker. However, it is obsolete and has no possible replacement.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: