{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the electrical burden for 9050JCK Timers?
Issue:
Consumption for type JCK timers coil

Product Line:
Relays and Timers

Environment:
9050 Type JCK Timers

Resolution:
The electrical burden can be found in Catalog 9050CT9601 (General Purpose Timers Type JCK Class 9050)
9050JCK11-59, 12-120 Vac/dc 2.0 VA
9050JCK11-59, 240 Vac 3.0 VA
9050JCK60-70, 12-120 Vac/dc 3.0 VA
9050JCK60-70, 240 Vac 3.2 VA

Schneider Electric USA