{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Do QBP-TM, QDP-TM, QGP-TM, and QJP-TM breakers come with mounting hardware?
Issue:
Does a QDP22200TM breaker come with mounting screws, and what are the part numbers?

Product line:
Circuit breakers

Resolution:
Yes. QBP-TM, QDP-TM, QGP-TM, and QJP-TM breakers include mounting hardware. The hardware is in a bag assembly inside the breaker carton when it ships. The bag assembly is part number 4812112257.

Schneider Electric USA