Search FAQs
What has replaced the obsolete HOMC40UC Homeline load center cover?
Issue:
Cross Reference for an obsolete load center cover
Product Line:
Homeline
Resolution:
Use catalog number HOMC42UC instead. This cover will have two more branch circuit twistouts than the HOMC40UC. Do not remove these extra twistouts. If they are accidentally removed, use (2) HOMFP to fill the open spaces.
Cross Reference for an obsolete load center cover
Product Line:
Homeline
Resolution:
Use catalog number HOMC42UC instead. This cover will have two more branch circuit twistouts than the HOMC40UC. Do not remove these extra twistouts. If they are accidentally removed, use (2) HOMFP to fill the open spaces.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: